Loading ...
Three examples of custom made gearboxes
Custom Gearboxes

Our experienced engineers always find the optimal solution for your application. No matter what the special requirements of your application, we can develop a custom made gearbox to match your needs.

PLE

Unparalleled: This planetary gearbox maintains its maximum efficiency even at the highest speeds.

View product
PLQE

The easy to install planetary gearbox absorbs high forces with low heat generation.

View product
PLPE

The cost effective planetary gearbox with the best torque-low heat performance.

View product
PLHE

This is progress: In this planetary gearbox, precision and cost effectiveness meet.

View product
PSBN

The high-performance precision planetary gearbox with helical teeth for a particularly quiet drive.

View product
PSN

The helical-toothed precision planetary gearbox for low-noise operation and high bearing loads.

View product
PLN

The perfectly sealed straight-toothed planetary gearbox delivers the maximum performance without ever losing the required stiffness.

View product
PLFE

The shortest planetary gearbox with the highest torsional stiffness and flange output shaft.

View product
PSFN

The precision planetary gearbox for maximum loads with particularly quiet drive and flange output shaft.

View product
PLFN

The precision planetary gearbox for maximum loads and the highest performance – fast and easy to install.

View product
WPLE

The versatile right angle planetary gearbox with lower weight and appealing cost effectiveness.

View product
WPLQE

The right angle planetary gearbox with universal output flange – flexible installation options and for high forces.

View product
WPLPE

The economical right angle planetary gearbox for particularly high forces – flexible installation options and lifetime lubrication.

View product
WPLN

The versatile right angle gearbox with spiral teeth for a quiet drive.

View product
WPLFE

The shortest right angle planetary gearbox with flange output shaft and maximum torsional stiffness.

View product
WPSFN

The shortest spiral-toothed right angle gearbox with flange output shaft and hollow shaft.

View product
WGN

The spiral-toothed right angle gearbox with hollow shaft – low noise levels and force-fit installation.

View product
HLAE

The unique planetary gearbox with certified hygienic design – ideal for reliable cleaning processes.

View product
Back to overview

Neugart affirmed as one of the best suppliers

For the fifth time consecutively, Neugart received the coveted Festo Supplier Elite Award. “We are delighted by Festo’s great recognition of our work,” said Bernd Neugart, Managing Partner of Neugart GmbH. “At the same time, however, we understand that this is not simply an incentive to continue down our path but to surpass the level of our achievements thus far.”

With this most recent Supplier Elite Award, Neugart joins an exclusive club of quality suppliers. To date, only a handful of suppliers – now including Neugart – have received Festo’s award at least five times. One of the reasons Neugart was recognized by Festo this year was because of their 100% delivery reliability as well as an exceptional PPM (parts per million) rate. Industrial customers demand a particularly low failure rate from their suppliers, which is then measured in PPM. Festo identified an impressive zero failure rate for Neugart products.

Festo and Neugart will continue to work closely together in the future, including on Festo’s efforts to place greater emphasis on the Chinese market. Neugart has already been active in China for 13 years, and, keeping in stride with Festo’s focused efforts, Neugart recently opened a new factory in Shenyang, China. “Our customers can expect the same quality of Neugart products regardless of where they are assembled,” said Bernd Neugart. “Our customers should expect nothing less.”

Do you have any questions?
Contact us.