- Home
- Knowledge & News
- News
Expanding the precision portfolio: the pro series
We are introducing a new performance class above our existing precision gearboxes with the new PSNpro, PSFNpro and PSBNpro series. These are based on new, innovative gear technologies and the use of new materials in production. The optimized tooth flank quality reduces point load peaks and enables higher torques to be transmitted with the same service life.
We have further developed our precision gearbox series using this technology. The result is the PSNpro, PSFNpro, and PSBNpro series, which set new standards in dynamic applications. In particular, cycle torque has increased significantly, enabling the pro series to rival and even surpass spur gearboxes. For applications involving frequent changes in load and direction, the pro gearboxes are therefore the obvious choice from the Neugart portfolio.
The pro gearboxes utilize the advantages of helical teeth to achieve excellent synchronisation. Transmission fluctuations between the input and output remain extremely low throughout the rotation of the output shaft. This visibly improves process quality and minimizes chatter marks in woodworking machines, for example. At the same time, the gearboxes operate at a particularly low noise level, even under high loads. This improves the system's acoustic properties and stabilizes the machine's overall performance.
Another area of development focused on reducing mass inertia, particularly in small frame sizes. Thanks to the consistent implementation of the modular principle, the input stage is now smaller than the output stage. This reduces the rotating mass, enabling faster acceleration and braking processes, as well as improving control quality in highly dynamic axes.
With the PSNpro, PSFNpro and PSBNpro gearboxes, we are opening a new chapter in precision gear technology. Combining our many years of experience in drive technology with innovation-driven development, we provide future-proof support for mechanical and plant engineering, robotics, and linear technology. This enables us to create reliable solutions that meet the requirements of modern drive technology and help our customers achieve higher productivity in the long term.
Let's stay in touch
Subscribe to our newsletter
Be the first to know about new products, trade shows, training dates and stay up to date.
Subscribe