Innovative Special Lubricant for the Economy Line
For our customers, we continually look for – and find – possible improvements even for fully developed products. The latest example: An innovative, special lubricant developed specifically for our planetary and right angle gearboxes. It immediately offers considerably improved protection against wear over an even wider temperature range.
The new "Klübersynth GE 14-112" lubricant is the result of a joint development project with the lubricant specialist Klüber Lubrication and has proven its capabilities in extensive tests. As a special grease for small gearboxes subjected to high loads, it contains specific additives formulated to exactly meet the requirements of planetary gearboxes. This new solution combines the competencies of both market leaders.
"The new development was an exciting challenge. Listen, advise, test – everything was focused on the requirements of Neugart. The result is exactly the right solution and incorporates numerous benefits for Neugart customers. The new solution addresses customer-specific requirements even more directly, since it offers an even expanded range of application", explains Jürgen W. Gehrig, Regional Sales Manager at Klüber Lubrication.
In practice, this change affects all Economy Line gearboxes (i.e. the series PLE, WPLE, PLQE, WPLQE, PLPE, WPLPE, PLFE, WPLFE, PLHE as well as their modifications) with the "Standard lubrication" option. The technical performance data at the reference point is guaranteed to remain unchanged. Customers who use these models benefit automatically from the advantages offered by this new lubricant. The change will take effect with the first shipment in 2021.