Back to overview

NCP 4.3: Neugart Calculation Program in a new version

Update for the configuration tool Neugart Calculation Program (NCP): In the new NCP 4.3 version the performance of the program has been improved further through improved multi-core usage of the processor. Above all, effective immediately the proven software will offer many additional features and optimizations - including better comparisons and rack-and-pinion drives.

Thanks to the expanded database, over 18,000 different motors are now available in NCP. Choices include not only servo motors, but also stepper motors. The motor design is carried out in a practical manner with graphical evaluation on the basis of the motor's characteristic curves. In addition, all Neugart wheels suitable for use with NGV gearboxes are included for traction drive applications in the new version.

Besides the expanded database, the application itself has also been optimized. For example, the comparison between theoretical design and actual data has become even easier. Drop-down menus minimize the effort required to prepare data when importing loads. At the same time, the accuracy of the motor trace load import is even greater than before, because the inertia of the motor and gear losses are now also included in the calculation. Further enhancements ensure even more reliability in the design.

Above all, newly designed details in NCP version 4.3 offer even greater convenience when using the program. New or occasional users in particular benefit from the intuitive usability and will find design examples for each application with detailed descriptions. By dragging files onto the program, the user can easily open files and add designs.
 

The new NCP 4.3 version is available for download free of charge here.