What is a Right Angle Gearbox?
Here, as the name suggests, we are concerned with the angle at which a gearbox operates. In a coaxial gearbox this angle is zero degrees. Most right angle gearboxes operate with an angle of 90 degrees between the input and output. Depending on how a right angle gearbox or right angle planetary gearbox is constructed, an axis offset may result —particularly when integrated with a servo motor or other compact drive systems. This configuration is often chosen for applications where space is limited or where a specific alignment of components is required.
Bevel Gearbox
Hypoid Gearbox
What Are the Most Common Right Angle Gearboxes?
The most common single-stage right angle gearbox types are bevel gearboxes and worm gearboxes. In many applications, however, right angle gearboxes are constructed by combining different gearing types.
Bevel gearboxes with intersecting axes can, for example, be constructed using straight-cut, helical-cut or spiral-cut gearing. So-called hypoid bevel gearboxes have spiral-cut bevel gearing. In these gearboxes, the axes cross with an axis offset. This has the advantage that the technically useful gear ratios are larger than with classic bevel gears , and that they allow for low backlash performance in motion-critical applications where continuous and precise operation is essential.
Right angle planetary gearboxes are often equipped with a standardized flange to ensure quick and secure mounting to servo motors and other precision equipment. For industries working with advanced motion control technology, this type of gearbox provides a reliable and efficient solution.
How Can Right-Angle Gearboxes Be Combined?
This can be done by using bevel gearboxes together with other types of gearboxes. Often this is done with planetary gearboxes. These can be connected upstream, as well as downstream. In either case, you have a great variety of total transmission ratios. Accordingly, there is also a wide range of applications for these gearboxes.
Choosing the Right Gearbox Series
Right angle planetary gearboxes are available in multiple series to suit different application needs. For example, our economy series offers a cost-effective solution for standard tasks, while the precision series is designed for applications that demand high accuracy and torque density. Application-specific series can be tailored to meet unique industry requirements, and each option can be configured for optimal speed, torque, and compatibility with your system. This ensures every customer finds the ideal gearbox solution for their system.
How Good is The Efficiency?
This is generally lower for bevel gearboxes than for coaxial gearboxes. Quite simply because high axial forces and radial forces are in play here. These forces are intercepted by the bearings, however. Nevertheless, there are losses, which are reflected in the lower efficiency.
Another shortcoming of these gearboxes is that they do not run as smoothly. In addition, they can only transmit lower torques than planetary gearboxes, for example.
In the special case of hypoid gearboxes, however, operation is smoother and the torques can be large compared to bevel gearboxes. However, this is "paid for" with a high load on the bearings in the bevel gear stage —especially in continuous operation with fluctuating dynamics.
When Are These Gearboxes Used?
Most often, when there is little space. But also if the application requires a special arrangement of input and output. For example, if the shaft is designed as a hollow shaft because cables are routed through it.
The advantages of right-angle gearboxes:
- They can be used when space is limited.
- They are compact in size.
- They can be easily combined with other types of gearboxes.
- As hypoid gearboxes, they run smoothly and can handle high torques.
- The shaft can also be designed as a hollow shaft.
- Designed to meet evolving customer demands and deliver a superior user experience.
The disadvantages of right-angle gearboxes:
- Their design is relatively complex.
- They have a lower efficiency than planetary gearboxes.
- Their running noise is higher than that of coaxial planetary gearboxes.
Our Gearbox Products
Frequently Asked Questions
Yes. Right angle planetary gearboxes are frequently designed for use with servo motors and are often equipped with standardized mounting flanges for easy integration into precision motion control systems.
A bevel gearbox changes the direction of power transmission using bevel gears, while a right angle planetary gearbox combines a right angle stage with planetary gearing. Planetary designs typically offer higher torque density, improved precision, and lower backlash for demanding automation applications.
This can be achieved by combining bevel gearboxes with other gearbox types, most commonly planetary gearboxes. These can be connected either upstream or downstream, allowing for a wide range of overall transmission ratios. As a result, these gearboxes are suitable for a broad variety of applications.
Efficiency is generally lower in bevel gearboxes than in coaxial gearboxes due to the high axial and radial forces involved. These forces are absorbed by the bearings, but some energy losses still occur, resulting in reduced efficiency.
Another limitation is that these gearboxes do not run as smoothly and typically transmit lower torques than planetary gearboxes.
In the case of hypoid gearboxes, operation is smoother and higher torques can be transmitted compared to standard bevel gearboxes. This comes at the cost of increased bearing loads in the bevel gear stage, particularly during continuous operation with fluctuating dynamics.
Let's stay in touch
Sign up to our newsletter
Be the first to know about new products, trade fairs, training dates and stay up to date.
Sign up