Application Story
100 lb+ Loads | 3 m/s Travel Speed | 4 Production Systems | 6–8 Years in Service
Every successful machine is the result of thousands of engineering decisions. One of the most important is selecting the right gearbox for the application. Watch how Bell-Everman balanced performance, reliability, service life, and value to engineer an overhead long-travel gantry system built for continuous production.
Customer Spotlight
Bell-Everman specializes in precision linear motion systems for demanding industrial automation. Founded in 1991, the company designs and manufactures its products in Southern California, serving industries including aerospace, semiconductor, biomedical, electronics assembly, CNC machining, and packaging.
For this project, Bell-Everman combined its expertise in long-travel gantry systems with Neugart planetary gearboxes to create a packaging automation solution that has been operating reliably in continuous production for more than six years.
Application at a Glance
| Application | Automated Tray Forming |
| Customer | Bell-Everman |
| Machine Type | Long-Travel Cartesian Gantry |
| Load | 110 lb (50 kg) |
| Speed | Up to 3 m/s |
| Operation | Three shifts per day |
| Time in Service | 6–8 years |
| Gearboxes | PLQE080, PLE060, PLE120 |
| Application | Automated Tray Forming |
| Customer | Bell-Everman |
| Machine Type | Long-Travel Cartesian Gantry |
| Load | 110 lb (50 kg) |
| Speed | Up to 3 m/s |
| Operation | Three shifts per day |
| Time in Service | 6–8 years |
| Gearboxes | PLQE080, PLE060, PLE120 |
THE CHALLENGE
Feeding Multiple Tray Formers Efficiently
Producing corrugated berry containers requires a continuous supply of cardboard blanks to multiple tray-forming machines. Manual loading can limit throughput, increase labor requirements, and make it more difficult to supply multiple tray-forming machines consistently.
Bell-Everman needed a solution capable of transporting heavy stacks of corrugated cardboard quickly, accurately, and reliably while serving multiple machines from a single automation platform.
The system also needed to provide long-term reliability under continuous operation while remaining cost effective for the machine builder.
THE SOLUTION
A High-Speed Long-Travel Gantry System
Bell-Everman designed an overhead Cartesian gantry to transport 100-pound stacks of corrugated cardboard to multiple tray-forming machines at speeds of up to 3 m/s. Neugart planetary gearboxes were selected throughout the system to deliver the right balance of performance, reliability, and value. Custom end-of-arm tooling was developed to securely handle stacks of corrugated cardboard while simplifying the surrounding material handling process.
Why a Long-Travel Gantry?
Compared with multiple articulated robots, a single overhead gantry can:
- Serves multiple tray-forming machines from one system
- Preserves valuable floor space with an overhead design
- Reduces safety guarding and maintenance complexity
- Provides fast, repeatable motion for continuous production
WHY THESE GEARBOXES?
This application did not require the lowest backlash or the quietest gearbox. Instead, Bell-Everman prioritized dependable performance, cost effectiveness, and long service life.
The selected Neugart gearboxes delivered exactly that balance.
Gearboxes Used
PLQE080
Used where reliable performance and cost efficiency were critical for continuous production.
PLE060
Provided dependable motion for supporting axes while maintaining excellent value.
PLE120
Handled larger loads within the gantry system while supporting demanding operating conditions.
Together, these gearboxes offered the performance required for the application without adding unnecessary cost.
THE SOLUTION
Proven in Continuous Production
The best measure of any automation system is how it performs in production.
Today:
- Four complete systems are operating in production.
- Each system has been running approximately three shifts per day.
- Installations have remained in service for six to eight years.
- The gearboxes continue to deliver reliable operation in a demanding packaging environment.
- One overhead gantry supports multiple tray-forming machines
For Bell-Everman, this demonstrated that dependable motion performance does not always require the highest-performance gearbox. Selecting the right gearbox for the application delivered an optimal balance of reliability and value.
“We've used Neugart gearheads for more than 20 years and trust them implicitly. We've never had a problem with quality, longevity, or durability.”
Mike Everman, CTO | Bell-Everman
Would you like to start a project together?
We would be happy to help you!
Neugart Sales Team
Let's stay in touch
Subscribe to our newsletter
Be the first to know about new products, trade shows, training dates and stay up to date.
Subscribe